TOSHIBA AMERICA BUSINESS SOLUTIONS EXPANDS WORKGROUP PRINTER OFFERING WITH THE INTRODUCTION OF THE POWERFUL E-STUDIO400P
New High-Volume Workgroup Printer Features Enhanced Performance, Expanded Document Handling and Wireless Printing Capabilities
IRVINE , California ( Jul 08, 2003 ) :
Toshiba America Business Solutions (TABS) continues to strengthen the technological breadth of its reengineered e-STUDIO workgroup printer line with the introduction of the flagship model - the powerful e-STUDIO400P monochrome, digital laser printer. Designed with expanded features and performance improvements targeted to meet the high-volume printing requirements of large workgroups, the e-STUDIO400P replaces Toshiba's workgroup printers, the e-STUDIO30P and the award-winning e-STUDIO40P, with enhanced paper handling and finishing capabilities, faster output speeds and new printing features.
Boasting a powerful 350 MHZ processor that breezes through documents at an impressive 40 pages-per-minute (ppm), the e-STUDIO400P offers a robust duty cycle of up to 200,000 pages-per-month, a first-print-out-time of only 10 seconds and an impressive 64 MB of RAM, which is expandable to a maximum 320 MB of RAM. These features, combined with true 1200 X 1200 dpi image quality, a new 802.11b (Wi-Fi) wireless printing option and a competitive price offering make the e-STUDIO400P the most comprehensive and affordable printing solution available on the market for today's demanding and sophisticated workforce.
"Ingenuity, quality, reliability and affordability are all hallmarks of Toshiba's e-STUDIO workgroup printer product line and the e-STUDIO400P is no exception," said Stephen Rhorer, director, Product Marketing, TABS. "By offering unparalleled image quality, incredible performance, fast output speeds, standard network connectivity and the added capability of wireless printing to enable busy executives to effortlessly connect to the information they need to keep business in motion, the e-STUDIO400P is yet another example of how Toshiba delivers leading-edge products and capabilities to drive business productivity to new levels."
Flexibile Connectivity Options
The e-STUDIO400P's modular architecture contributes to its functionality in the workplace, enabling users to effortlessly tailor it to address a range of business needs. In addition to offering standard PostScript™ 3 and PCL 6 emulations, 10/100BaseT network connection and USB port, the e-STUDIO400P is the first Toshiba printer to offer a Wi-Fi wireless printing option. With Wi-Fi printing capabilities, the e-STUDIO400P offers users limitless opportunities to enhance business productivity by eliminating cumbersome wires, making wireless connectivity to printers and accessibility to crucial information, seamless. Mobile users can now easily access the e-STUDIO400P without having to worry about locating an open network connection or printer cable. In addition, the e-STUDIO400P supports a dynamic range of operating systems including Mac OS 8.6 or higher, Windows 9x, NT 4.0, 2000, Me and XP, as well as Novell Netware 3.x, 4.x and 5.x, making it the reliable printing solution capable of effectively handling any project and environment.
Superior Document Handling Capabilities
In today's connected world, information is delivered at light speed and is processed in increasing volumes. The e-STUDIO400P offers a large paper, input and output capacity to address these high-volume, high-demand environments. In addition to an impressive input capacity of 4,100 sheets, the e-STUDIO400P offers a standard 500-sheet drawer and a 100-sheet bypass, with options including a 500-sheet drawer and a 2,000-sheet drawer. To enable envelope printing, the e-STUDIO400P offers an optional envelope feeder that simplifies the process of printing envelopes in larger quantities. With output options that include capacity up to 3,000 sheets, a 650-sheet output expander and a 1,850-sheet high capacity output stacker (HCOS), long job runs can be handled with ease, and a StapleSmart Finisher enables users to efficiently and easily produce finished document sets on the spot.
With its expanded document handling and finishing capabilities, the e-STUDIO400P is an excellent complement to other e-STUDIO multifunction product (MFP) solutions and can help offset multiple printing jobs to further enhance business efficiency.
The e-STUDIO400P comes standard with letter and legal-sized paper handling capabilities and accommodates a variety of media types including plain paper, letterhead, envelopes, cardstock and transparencies. A 21,000-yield starter cartridge also comes standard and a 32,000-yield replacement cartridge also is available in either a disposable or lower cost Use-and-Return type for added convenience.
The e-STUDIO400P is available through Toshiba's nationwide network of dealers for the suggested list price of $1539 (USD).
About Toshiba America Business Solutions
Toshiba America Business Solutions, Inc. (TABS) manages product planning, marketing, sales, service support and distribution of copiers, facsimiles, multifunction printing products, network controllers and toner products throughout the United States, Latin America and the Caribbean. Headquartered in Irvine, Calif., TABS comprises four divisions: the Electronic Imaging Division, Toner Products Division, Document Solutions Engineering Division and TOPAC, a subsidiary which operates a network of office equipment dealers.
Named the most favored manufacturer in seven of the past eight years by the Business Technology Association (BTA), Toshiba's entire product line, customer support and marketing distribution policies are a marker for the industry. Among the many other awards garnered in recent years, Toshiba was named the "Copier Manufacturer of the Year" by the Marketing Research Consultants (MRC) in 1997, 1998, 2001 and 2002 and received the CIO Web Business award for its leading edge intranet site in 1998, 1999 and 2000.
TABS is an independent operating company of Toshiba Corp., the fifth largest electronics/electrical equipment company and the world's 77th largest company in terms of sales. Toshiba Corporation is a world leader in high technology products with more than 300 major subsidiaries and affiliates worldwide. Fiscal year revenue in 2002 was approximately $47 billion.
For more information on Toshiba copier, facsimile and printer products, or for a local dealer, call 1 800 GO TOSHIBA or visit the TABS Web site at www.copiers.toshiba.com.