TOSHIBA AMERICA BUSINESS SOLUTIONS INC. INTRODUCES e-STUDIO™250CP COLOR PRINTER INTO WORKGROUP COLOR LINE
Color Laser Printer Combines High Performance, Quality Images and Affordability
IRVINE , California ( Aug 10, 2005 ) :
Toshiba America Business Solutions Inc. (TABS) today introduced the latest addition to its workgroup color laser printer line, the e-STUDIO™250CP. Toshiba’s newest color printer delivers print speeds of 25 pages-per-minute (PPM), a fast first print out time of just 13 seconds in monochrome and 15 seconds in color, and crisp 4800 dpi image quality, all at an affordable price.
“The e-STUDIO250CP makes the use of color in the workplace more attainable by providing an affordable solution that can satisfy full or spot color tasks, such as production of charts, graphs, presentation materials, marketing collateral and internal communication tools,” said Steve Rhorer, director, Product Marketing for TABS. “The e-STUDIO250CP is ideal for corporate environments with mid- to high-volume workgroups needing color printing and finishing capabilities.”
Sharp, High-Quality Color Images
Incorporating a 600 MHz processor, image quality tops the e-STUDIO250CP’s impressive list of features. In addition to the standard 1200 x 1200 dpi resolution, the e-STUDIO250CP offers enhanced 4800 dpi image quality for advanced halftone-screening methods that result in improved image quality. This feature also reduces the time to print by using less memory for faster spooling. Additionally, an automatic color correction control system produces clean, sharp text with solid and bright colors.
Along with a monthly duty cycle of 100,000 pages per month, the e-STUDIO250CP offers long toner life of 6,000 yield starter cartridges for both black and color toner. Furthermore, long life 15,000 yield replacement cartridges are available, which means users do not have to worry about constantly replacing supplies. In addition, to help lower the cost of operation and increase the life of toner supplies, the e-STUDIO250CP features a Color Saver function that reduces the saturation in all color levels.
Versatile Paper Handling
The e-STUDIO250CP is designed to fulfill a variety of printing requirements, allowing users to print on transparencies, envelopes, labels and card stock up to 110-pound index. In addition, the e-STUDIO250CP can handle letter and legal paper sizes and comes standard with a 500-sheet drawer and a 100-sheet bypass. An optional 500-sheet drawer, 2000-sheet drawer, Duplex unit, Envelope feeder, 5-bin mailbox and Output expander also are available. Business color users that need to produce a wide range of finished document sets can take advantage of an optional 3000 Sheet Finisher, offering stapling, hole punch and job offset features.
Complete Network Compatibility
The e-STUDIO250CP is compatible with all major network operating systems, including Windows 98 SE, NT4.0, 2000, ME, XP, Server 2003, Novell Netware 3x, 4x, 5x, 6x and Mac O/S 8.6 or later. To meet the growing demand of connectivity in the business environment, the e-STUDIO250CP comes standard with a 10/100BaseT network interface and a USB 2.0 connection. An IEEE 802.11g wireless option also is available to accommodate mobile office users.
The e-STUDIO250CP is now available through Toshiba’s nationwide network of dealers for a suggested list price of $2,099 (USD).
About Toshiba America Business Solutions Inc.
Toshiba America Business Solutions Inc. (TABS) manages product planning, marketing, sales, service support and distribution of copiers, facsimiles, multifunction printing products, network controllers and toner products throughout the United States, Latin America and the Caribbean. Headquartered in Irvine, Calif., TABS has four divisions: the Electronic Imaging Division, Toner Products Division and Document Solutions Engineering Division; and Toshiba Business Solutions (TBS), which operates a national network of wholly owned subsidiaries.
Named the most favored manufacturer in seven of the past eight years by the Business Technology Association (BTA), Toshiba’s entire product line, customer support and marketing distribution policies are markers for the industry. Among the many other awards garnered in recent years, Toshiba was named the “Copier Manufacturer of the Year” by the Marketing Research Consultants (MRC) in 2005, 2004, 2002, 2001, 1998 and 1997, was named to the CIO 100 for being one of the top 100 “agile” companies in the world in 2004, and received the CIO Web Business award for its leading edge intranet site in 2000, 1999 and 1998.
TABS is an independent operating company of Toshiba Corporation, the seventh largest electronics/electrical equipment company and the world's 62nd largest company in terms of sales. Ranked by Fortune magazine as the 8th Most Admired Electronics Company in America and 9th Most Admired Electronics Company in the World, Toshiba Corporation is a world leader in high technology products with more than 300 major subsidiaries and affiliates worldwide. Fiscal year revenue in 2004 was approximately $55 billion.
For more information on Toshiba copier, facsimile, multifunction printing products, network controllers or toner products, or for a dealer in your area, call 1-800-GO-TOSHIBA or visit the TABS Web site at www.copiers.toshiba.com.