TOSHIBA AMERICA BUSINESS SOLUTIONS INC. LAUNCHES THE e-STUDIO™523/603/723/853 MULTIFUNCTION SERIES TO BUSINESSES
Windows Vista Support, XPS Print Support and Enhanced Security Integrated into Proven High-Volume Document Imaging Family
IRVINE , California ( Jan 23, 2008 ) :
Toshiba America Business Solutions Inc. (TABS) raised the bar for monochrome multifunction products (MFPs) today by announcing the new and improved
e-STUDIO™523/603/723/853 and e-STUDIO™523T/603T/723T series nationwide. Built on the robust platform of the popular e-STUDIO520/600/720/850 family of MFPs, the new line of high-speed, large-volume MFPs feature expanded security elements and encryption, support for the Microsoft® Windows Vista™ operating system and enhanced XPS printing options. The e-STUDIO523/603/723/853 series incorporates exceptional image quality, high-speed printing and multiple paper source options, making it the perfect choice for high-volume production environments.
The e-STUDIO523T/603T/723T family shares all the same product features as the e-STUDIO523/603/723/853 series, with the added convenience of tandem 1,250-sheet letter paper cartridges, effectively doubling the printing output capacity between paper refills in the same MFP footprint.
“Toshiba’s e-STUDIO523/603/723/853 and their ‘T’ counterparts are built upon a proven productivity and reliability platform that our large workgroup monochrome MFPs have become renown for,” said Joe Contreras, director, Product and Solutions Marketing, TABS. “By incorporating Windows Vista support and extended security into these fast, efficient and highly versatile machines, we are empowering businesses with the ability to meet all their high-volume print needs.”
Proven Technology, Outstanding Image Quality and Impressive Performance
The e-STUDIO523/603/723 and e-STUDIO523T/603T/723T MFPs feature a high-speed, single-beam laser-imaging unit, while the e-STUDIO853 uses a dual laser-beam design, delivering pin-point print accuracy across the family of MFPs for every single copy. An 8-bit scanner module and up to 2,400 x 600 dpi output ensures that scans and copies are as clean as the original, while not compromising production speed. Standard in both MFP lines is the Toshiba Serial Filter, which produces crisp, sharp text and line-art, while maintaining deep black fills.
The Toshiba e-STUDIO523/603/723 and their T equivalents offer print speeds of 52, 60 and 72 pages-per-minute respectively, while the e-STUDIO853 prints at a blistering 85 pages-per-minute, ensuring efficient document output throughout the product line. All models scan at 71 scans-per-minute at 600 dpi when copying, and 83 scans-per-minute at 300 dpi when scanning to file. The e-STUDIO853 features a first-copy-out-time (FCOT) of less than 3.5 seconds, with rest of the product family close behind with a less than four second FCOT.
Incorporating Toshiba’s e-BRIDGE single-board architecture, the e-STUDIO523/603/723/853 series uses a single circuit board to control copying, printing, scanning and other functionality to decrease memory overhead and improve print time. Additionally, a dual-speed paper handling system slows down the paper while it passes through the process unit and makes up the speed elsewhere to maintain performance.
Native Windows Vista Support
Working closely with Microsoft, Toshiba’s new e-STUDIO523/603/723/853 and e-STUDIO523T/603T/723T family of products provide Windows Vista-specific printing enhancements in the form of XPS Print Path drivers, Windows Color System support and Windows Vista WS print and scan support, while remaining 100 percent backwards-compatible with existing deployments. This XPS format integration offers full printer functionality and enables users to print 2007 Microsoft Office system documents directly to the MFP without the wasted overhead of file conversion.
Improved Security Features
Continuing the legacy of being one of the most protected MFPs on the market, the e-STUDIO523/603/723/853 and e-STUDIO523T/603T/723T series offer advanced security features, including support for IPv6, IPSec, SSL, SNMPv3, 802.1x authentication, providing secure management and network communications. Additionally, the entire product family includes Encrypted PDF, allowing users to add a password when creating scanned PDFs, to prevent unauthorized viewing or printing.
The e-STUDIO523/603/723/853 series is now available through Toshiba’s nationwide network of dealers for suggested list prices of $18,495, $22,995, $27,995 and $35,995 respectively. The e-STUDIO523T/603T/723T series also is available through Toshiba’s nationwide network of dealers for suggested list prices of $18,995, $23,495 and $28,495 respectively. To find the authorized Toshiba dealer nearest you, or for more information on Toshiba’s wide line of document imaging products, solutions and total print management offerings, please visit www.copiers.toshiba.com.
About Toshiba America Business Solutions Inc.
Toshiba America Business Solutions Inc. (TABS) manages product planning, marketing, sales, service support and distribution of copiers, facsimiles, multifunction printing products, network controllers, and toner products throughout the United States, Mexico, Brazil, Latin America, and the Caribbean. Headquartered in Irvine, Calif., TABS has four divisions: the Electronic Imaging Division; the Toner Products Division; the Document Solutions Engineering Division; and TOPAC U.S.A., Inc., dba Toshiba Business Solutions (TBS), a wholly-owned subsidiary corporation of TABS, that operates a network of wholly-owned office equipment dealers throughout the United States.
Named the most favored manufacturer eight times by the Business Technology Association (BTA), Toshiba’s entire product line, customer support and marketing distribution policies are markers for the industry. Among the many other awards garnered in recent years, Toshiba was named the “Manufacturer of the Year” seven times by Marketing Research Consultants (MRC), and has twice been named to the CIO 100 for being among the top 100 “bold” (2005) and “agile” (2004) companies in the world.
TABS is an independent operating company of Toshiba Corporation, the seventh largest electronics/electrical equipment company and the world's 91st largest company in terms of sales. Ranked by Fortune magazine as the 10th Most Admired Electronics Company in the World, Toshiba Corporation is a world leader in high technology products with more than 300 major subsidiaries and affiliates worldwide. Fiscal year revenue in 2006 was approximately $60 billion.
For more information on Toshiba copiers, facsimiles, multifunction printing products, network controllers or toner products, or for a dealer in your area, call (800)-GO-TOSHIBA or visit the TABS Web site at www.copiers.toshiba.com.